FB#.SIGNALAMPLITUDE

Description

This parameter returns the measured signal amplitude of a connected resolver or sine/cosine encoder.

It is only available on the following encoder types:

  • Sine Encoder with Halls
  • Sine Encoder without Halls
  • EnDat Analog
  • Resolver
  • HIPERFACE
  • BiSS-B with SinCos

These commands are not recordable on FB1 and FB2.

For recording on FB1 and FB2, see FB#.MONITOR#.SOURCE and FB#.MONITOR#.DATA.

Example

Usage

The signal amplitude measurement is used to detect if the sine/cosine signals from the encoder have an acceptable amplitude. If the amplitude is outside the acceptable range, a fault is thrown.

The signal amplitude is approximately equal to the length of the sine/cosine signal vector: sqrt(sin2 + cos2). If the signal amplitude changes with angle, the sine and cosine signals have different amplitudes.

Target signal strengths and acceptable ranges are in the table below:

Encoder Nominal Maximum Minimum
Resolver 3.5 Vms 3.86 Vrms 2.25 Vrms
Sin/Cos 0.3536 Vrms (1 V pk-pk) 0.495 Vrms (1.4 V pk-pk) 0.1767 Vrms (0.5 V pk-pk)

Code

--> FB3.SIGNALAMPLITUDE
1.123 [Vrms]

Versions

Action Version Notes
Implemented 02-00-02-000  

General Information

Type

Read Only

Units

Vrms

Range

N/A

Default Value

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB1.SIGNALAMPLITUDE

3500h

25h

Signed32

-

1000:1

Read only

No

FB2.SIGNALAMPLITUDE

3501h

25h

Signed32

-

1000:1

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30260

1

30260 (0x7634)

FB1.SIGNALAMPLITUDE

Signed32

Read Only

Yes

30261

1

30261 (0x7635)

FB2.SIGNALAMPLITUDE

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.SIGNALAMPLITUDE

30260

Float

Read Only

-

FB2.SIGNALAMPLITUDE

30261

Float

Read Only

-

Related Topics

FB#.MONITOR#.DATA

FB#.MONITOR#.SOURCE